2/26/2016 10:25 AM | |
Posts: 11 Rating: (0) |
Thx Cristoph, but you don't know why if I install GSD file for 2BA10 I can't find it in HW. |
2/26/2016 10:33 AM | |
Joined: 5/12/2006 Last visit: 6/7/2024 Posts: 22255 Rating: (2986) |
Hi, have you read the post from me? PROFIBUS DP -> Additional Field Devices -> I/O -> ET200M If have tested this with the GSD File "IM153-2BAx0_HF_DPV1_H_12IO.zip" from: https://support.industry.siemens.com/cs/ww/en/view/113498 Regards |
2/26/2016 11:00 AM | |
Posts: 11 Rating: (0) |
Hi, Yes, I found 2BA02 and I instal GSD File "IM153-2BAx0_HF_DPV1_H_12IO.zip" but 2BA10 is not listed. |
2/26/2016 11:26 AM | |
Joined: 5/12/2006 Last visit: 6/7/2024 Posts: 22255 Rating: (2986) |
Hello, is listed with "6ES7 153-2BA*0-0XB0", the wildcard "*" is suitable for the "1".
Christoph |
Follow us on