4/13/2016 10:01 AM | |
Posts: 23 Rating: (0) |
Hi All, I'm Newbie in new Siemens controllers and if possible i need your help. We bought CTX310 (Main spindle Upper turret and driven tools) with Sinumerik 810D Slimline with Driven tools and i meet few problems when trying to run machine program, actually when i want to run program in Auto mode i should enable feed and spindle but i can not find softkey on controller to do achieve this (as in older sinumerik controllers). and in auto mode program is loaded and wont start because feed is not enabled and i assume turning spindle. For Feed warning i just recieve no feed enable signal like in zipped file bellow. Second is spindle, whatever i choose spindle to be active (S1 or S4) it pop up error that tool switch is not engaged and im not able to start spindle in manual or MDI mode. All pictures are attached inside Zipped file Thanks in advance Best Regards
AttachmentDSC_0054 (3).zip (131 Downloads) |
Follow us on