4/18/2017 10:36 AM | |
Joined: 4/24/2006 Last visit: 5/28/2024 Posts: 8659 Rating: (1154) |
Hello, Perhaps the following link might help: Tool collection for converting data types Best regards, Wizard |
This contribution was helpful to1 thankful Users |
4/18/2017 12:04 PM | |
Joined: 10/23/2015 Last visit: 2/18/2024 Posts: 159 Rating: (2) |
Tks, unfortunatly, i didnt find anything intersting about there, thanks |
4/18/2017 1:14 PM | |
Posts: 15 Rating: (1) |
In Standard Library, IEC Function block, take the FC 16 |
4/18/2017 6:51 PM | |
Joined: 9/27/2006 Last visit: 5/28/2024 Posts: 12257 Rating: (2668)
|
Hello frahi; I have used IEC functions in many programs and have never had the type of problem you show. What I would suggest, for a trial, would be to reprogram FC 16 without using TEMP variables; use M-Flags or DB registers. There is a basic issue with TEMP variables: the local stack (where TEMP varibles are located) is shared by all the FC/FBs in your program, and unless you specifically initiate them with known (and valid) values in your FC you have no idea what they contain. This often leads to very strange results, as you can see in these various discussions on the forum: Collection of threads on TEMP variables initiation. Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on