7/16/2017 6:48 PM | |
Posts: 1 Rating: (0) |
Hello First of all as a "newbe" i`d like to say Hello to every User :) I`d like to ask about connection of key-switch (S36 on photos) on the cotrol panel of sinumerik system 3M. I`m trying to rebuild/learn about CNC control units. Currently i`m not able to choose any "manual" mode on the selector switch. It stays on Data input up to MDI-SE-TE. Board model:GE.548188.0002.00 Here are the pictures Second thing i`d like to ask is transmission between PC <-> Sin_3M. I was able to transmit from system to PC %program all at once into one file. When i choose for example one program lets say%1234 i`ve got error 512. Also i wasnt able to send programs from the PC to machine. Thanks in advance for any help. Regards Pawel AttachmentPictures.zip (49 Downloads) |
Last edited by: Jen_Moderator at: 7/18/2017 11:33:03 AMAdded Pictures as an attachment. |
|
Follow us on