6/1/2016 8:24 AM | |
Posts: 4 Rating: (0) |
hi. i am using cpu 414 5h. when ever i try to download the program its showing following error: E:the available load memory insufficient for the program download (exceeded by approx. 28%) please increase load memory. pleas help me. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/1/2016 9:40:52 AMNew subject after splitting Last edited by: raminfathi at: 6/1/2016 10:15:14 AM |
|
6/1/2016 9:24 AM | |
Joined: 10/7/2005 Last visit: 5/29/2024 Posts: 3007 Rating: (1049)
|
Hello raminfathi A 414-5 H (6ES7414-5HM06-0AB0) has 4MB of inbuilt work memory but only 512kB of inbuilt load memory. Assuming you have NOT yet expanded the CPU's load memory, your solution is to do so by adding at least a 4MB RAM card to give you a total of 4.5MB Load memory (Load memory can be expanded and is ideally larger than the inbuilt non-expandable work memory, see also THIS and THIS FAQ for more). I hope this helps |
Cheers |
|
6/1/2016 10:26 AM | |
Posts: 4 Rating: (0) |
thank you |
6/7/2016 3:55 AM | |
Joined: 10/7/2005 Last visit: 5/29/2024 Posts: 3007 Rating: (1049)
|
Suggest you read the reply again I gave above. |
Cheers |
|
Follow us on