11/4/2017 10:15 AM | |
Posts: 241 Rating: (1) |
|
11/5/2017 2:47 PM | |
Joined: 9/27/2006 Last visit: 6/10/2024 Posts: 12260 Rating: (2670)
|
Hello Hamed; In all honesty, I cannot tell from the screenshot you provided what equipment you are using to read the load cells. If the equipment and functions are provided by Siemens to manipulate and normalize the values read from the load cells, with the name of the input Equipment maybe someone on the forum can help. If these are specialized functions devised by Siemens programmers, maybe the Siemens Support guys can help. Try a support request. But if they are non-standard blocks devised by an application team in the field, we cannot say much until we see the code, if possible. If you want to understand why these functions are necessary to manipulate the read values of a load cell, there are many articles on the subject, such as these ones: Hope this helps, Daniel Chartier AttachmentBridge Measurement Systems - Texas Instruments.pdf (21 Downloads) |
Last edited by: dchartier at: 11/5/2017 2:48:21 PMLast edited by: dchartier at: 11/5/2017 6:31:10 PMLast edited by: Jen_Moderator at: 11/6/2017 1:33:17 PMAdded PDF as an attachment. |
|
This contribution was helpful to2 thankful Users |
Follow us on