3/13/2017 3:38 AM | |
Posts: 5 Rating: (0) |
Please help me! My screen Logo!OBA8 have only 3 menu: + Setup + Network + Diagnotices I realy don't known Factory Reset. Please help me Thank you so much ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/13/2017 10:52:11 AMContact data deleted Last edited by: Min_Moderator at: 3/13/2017 10:54:01 AMNew subject after splitting |
|
3/13/2017 6:25 AM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33167 Rating: (4098)
|
A factory reset is only available with the LOGO! 8.FS04. With the 0BA8.Standard there is no factory reset. The minimized menu is created by switching on the operator mode. To enter Administrator mode, you must enter a password. The attachment contains an extract from the manual, where the procedure is described. AttachmentLOGO! 8 Soft manual 0BA8 2016_07 (FS4) sides 69-71.pdf (2646 Downloads) |
Last edited by: ixo65 at: 5/17/2017 8:33:39 PMContact data user nguyenquockhoa removed. |
|
This contribution was helpful to3 thankful Users |
5/17/2017 8:14 PM | |
Posts: 1 Rating: (0) |
Thanks for the help |
This contribution was helpful to1 thankful Users |
11/10/2017 11:21 AM | |
Posts: 2 Rating: (0) |
Thanks! |
Follow us on