1/27/2015 6:04 AM | |
Posts: 10 Rating: (0) |
Hello! Normally You have to recommission the motor using start-up tool and enter the appropriate motor MLFB during this procedure. As soon as this is a Siemens motor, all parameters would be generated automatically. Another way is to enter drive parameter p1102 manually (please see attached pdf). Then I would recommend to make the drive optimization (tuning) procedure if the quality of the movements would be unappropriate..
AttachmentFunction Manual Drive Functions - FBA.pdf (152 Downloads) |
This contribution was helpful to1 thankful Users |
4/16/2018 12:16 PM | |
Joined: 6/19/2017 Last visit: 5/2/2024 Posts: 7987 Rating: (163) |
New question published by dadkhah is split to a separate thread with the subject 1FK7063-5AH71-1GB3 and 6SN1123-1AA00-0CA1: Need help with wiring and the test procedure. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on