10/26/2018 3:19 PM | |
Joined: 2/17/2012 Last visit: 2/10/2024 Posts: 3 Rating: (0) |
hı I'm trying to install the 840d sl unit. But I can't get rid of the 27032 27033 alarms. I am adjusting the installation according to the s3 and s4 key procedure in ncu. I had installed the PLC after the previous installation before the NC never worked smoothly in the machine. But my current burden is constantly coming to these alarms. In the archive there is an integrated file, including nc plc and mmc, but it takes too long and does not open. How do you think I should load? ------------------------------------------------------------------------------------------ |
Last edited by: nurkon at: 10/26/2018 3:33:49 PMLast edited by: Jen_Moderator at: 10/26/2018 3:36:33 PMNew subject after splitting |
|
10/26/2018 3:35 PM | |
Joined: 2/17/2012 Last visit: 2/10/2024 Posts: 3 Rating: (0) |
There is a problem of copying:) Thank you for your kindness. |
10/26/2018 4:16 PM | |
Joined: 10/17/2007 Last visit: 6/2/2024 Posts: 3999 Rating: (345)
|
Install? do you mean you restore the back up of the machine or you make a new machine? if your restore back up data to recover your machine, you should use exactly original data of the that machine. specially like your 840D sl system with safety integrated. the 2 alarms already showing you one MD is wrong, if you cannot make it correct , you need to find out which NC back up is good. the archive file is for back up and reloading don't try to open it. just load it
|
If you like my comments please |
|
Follow us on