5/14/2019 9:31 PM | |
Joined: 6/1/2017 Last visit: 5/8/2024 Posts: 13 Rating: (0) |
Hi everyone I take a machine backup using simetic manager V5.5 sp4 .Problem is created when I find analog addresses PIW & PQW in cross reference but nothing to show and then I also open every FCs And FBs but also failed to find any PIW & PQW . Program is in STL Indirect pointer addressing and I am weak in pointer indirect addressing. please anyone open my attached program and go to HW configuration then see profibus adress 60 & 70 then see analog address and then find these addresses in program. pointers are mostly used FBs 80 to onward & FCs 80 to 89. Please I am in trouble help me as soon as .I take a project but nothing to understand . My final aim is to change analog addresses in HW config & in program . please check my attached program. THANKS AttachmentRanatex_.zip(0 Downloads) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/15/2019 06:42:31New subject after splitting |
|
5/14/2019 10:18 PM | |
Joined: 9/21/2012 Last visit: 6/6/2024 Posts: 3964 Rating: (449) |
Please be so Kind and don't post twice or more for the same Problem. Thanks |
5/15/2019 6:49 AM | |
Joined: 6/19/2017 Last visit: 6/6/2024 Posts: 8149 Rating: (165) |
Closed cause question posted twice. The second thread with the subject Can't find any PIW & PQW is published within the conference STEP 7 / STEP 7 Lite. Best regards Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on