4/30/2020 9:18 AM | |
Joined: 9/21/2012 Last visit: 2/1/2024 Posts: 4 Rating: (1) |
Dear all, I will post here as I don't want to add one more similar thread to a probably existing one. I own a CPU 314 6ES7 314-1AE04-0AB0 . I know that I cannot program this CPU with TIA PORTAL (correct?) , however, I also cannot find this CPU in the catalogue of Simatic Manager STEP 7 V.5.5+SP4 that I use :) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/30/2020 11:32:55New subject after splitting |
|
4/30/2020 12:32 PM | |
Joined: 9/21/2012 Last visit: 6/16/2024 Posts: 3973 Rating: (451) |
Have you installed all HW Updates in Hardware configuration? Because i can see this CPU in my HW catalog. |
4/30/2020 12:56 PM | |
Joined: 9/27/2006 Last visit: 6/16/2024 Posts: 12260 Rating: (2671)
|
Hello Dimmitri; Actually, your CPU is in spare part mode, no longer in production. This is the technical data of your S7-314. https://support.industry.siemens.com/cs/us/en/pv/6ES7314-1AE04-0AB0/td?dl=en The software required to program it is Step 7 v5.0, as per its technical data. So it should be accessible through the Step 7 v5.4 hardware catalog, as mentioned by Hati. Please check again in your HWConfig selections. If you cannot find your model. Please send us a screenshot of your hardware selections, showing the closest available part numbers in your HWConfig. Hope this helps, Daniel Chartier |
Follow us on