1/18/2020 7:48 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Hello, Please refer attached sheet & follow below points. 1. First clear NC & PLC data as per attached sheet. Follow the steps & check LED blinks as mentioned which confirms data clear. 2. Reload data sequentially as mentioned, pay attention to set password & after setting it, on screen at below MANUFACTURE level set is displayed. Then reload data as stated. Pay attention on LED status. The procedure is not complex, only patience & attention is required. If during loading any error occures, take snap shot & revert. HTH. Attachment840d PL NC___PLC_Data_Clear & restore procedure.pdf (430 Downloads) |
This contribution was helpful to3 thankful Users |