8/28/2018 2:45 PM | |
Posts: 1 Rating: (0) |
Hi Im Daniel i got a sinumerik 808d milling with spindle 8000rpm and manual gear box im working in iso Mode The point is i order spindle by NC Go to s4000 and only teach 1200rpm..in controller show It Manufacture said need to active m42 gear milling We put m42 in mdi M6706d6 M03 S2500 M42 M30 And give error 022110 gear is not same as active We need to work in more rpm Helpme how i could? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/29/2018 8:25:35 AMNew subject after splitting |
|
8/29/2018 6:00 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Please write sequence correctly, first M42 i.e. gear change & then spindle rpm. M42 M03 S2500 Check. |