8/24/2010 10:58 PM | |
Posts: 71 Rating: (0) |
HI, Attachment840D sl HW.zip (510 Downloads) |
8/25/2010 10:36 AM | |
Joined: 1/19/2008 Last visit: 6/3/2024 Posts: 984 Rating: (63) |
Hi, Same problem only the profinet version on the cd I'll attach it below. Hopefully you can save it. If not drop me your email in a private message Note I have changed the file extension to zip to allow the upload on the Siemens system. Change the file extension to GSD it is NOT a zip file. Pee AttachmentSIEM80A2.zip (622 Downloads) |
8/25/2010 4:15 PM | |
Posts: 71 Rating: (0) |
Thank you Pee Icouldnt open the file. I sent you a private massage contain my Email so you can Emailed me the file. Regards Tarik |
8/27/2010 6:06 AM | |
Posts: 2964 Rating: (481) |
Hello.... Could check the addressing on the PP module? The addresses are set using the DIL switch S1 on the PP module..... I am attaching you the document of the same for the referernce..... Check it out.... Regards, Ekalavya Attachmentpp module.pdf (497 Downloads) |
8/27/2010 10:11 AM | |
Joined: 1/19/2008 Last visit: 6/3/2024 Posts: 984 Rating: (63) |
Hi, Make sure you've added the I/O into the hardware !. |
9/5/2010 5:19 PM | |
Posts: 71 Rating: (0) |
Dear Pee Iattached the information that you ask. about your question ,did you ask about thePP i/o cofiguration in basic PLC program. Regards Tarik AttachmentTEMP.zip (267 Downloads) |
9/7/2010 5:43 PM | |
Joined: 1/19/2008 Last visit: 6/3/2024 Posts: 984 Rating: (63) |
Now I'm totally confused. When I click on the pp module and insert it onto the profibus the hardware box has :- PP Input /Output Module in the box and displays part number 6FC5 611-0CA01-0AA0. Your picture is showing an I/O manager This only gives you an interface you then have to put the A/E 6/9 A222, E212121 unit inside it. Attachmenthw1.zip (280 Downloads) |
Follow us on