8/29/2019 2:57 PM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32949 Rating: (4072) |
1.1 What has Changed Compared to Version STEP 7 V5.6 SP1? HW Config ·The installation of HSPs is now possible using the command line call via the HSP installer. You can find more information in the help on configuring the hardware in topic "Installing HW Updated via the Command Line". ·The operation of a DP/FF-Link downstream from an IE/PB-Link V3.1 is now possible. ·A configuration in RUN is now once again possible for specific configurations that were downloaded to the CPU with STEP 7 V5.5 SP4 HF9. ·As of this Hotfix: The behavior when loading the hardware configuration when test functions are still active, e.g. "Monitor/control" has been improved. NetPro ·The output of warnings during compilation in NetPro has been improved. Report System Error ·Generating 'Report System Error' has been improved. Download Hotfix 5 STEP 7 V5.6 SP1 / STEP 7 Professional 2017 SR1 |
This contribution was helpful to3 thankful Users |