6/13/2022 2:05 PM | |
Joined: 6/13/2022 Last visit: 6/21/2022 Posts: 1 Rating: (0) |
Hello, I am having the same fault on my Weiler E70. On the desplay the fault showing is "spindle or 4-way switch defective". When I push the NC reset the fault then changes to "Channel 1 axis Z/Z1 hardware limit switch+" When I go into the alarm list. I then see the 400552 fault on DP Bus alarm. There are other multiple faults including 700503 Overload 230V supply. Any suggestions on what I can do to get my machine back online and running would be helpful. Thank You Combatcommo ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 06/13/2022 19:54:20New subject after splitting |
|