9/30/2011 11:42 AM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating: (37) |
Hello, Could you tell the excat alarm number with the System type. |
Regards, |
|
9/30/2011 2:57 PM | |
Posts: 2964 Rating: (481)
|
Hello.... Check have you entered password..... Keep PLC S4 position 2 and then reload your PLC archive backup Regards, Prakash |
9/30/2011 3:06 PM | |
Posts: 23 Rating: (0) |
Ekalavya sir i followed attached procedure as suggested by you.......plz check attached procedure and if there is mistake in help me in this...... one more thing As per procedure we cleared and reload the plc but according to step 3 of attached procedure i.e. when we turned s4 to 2 - 3 - 2 position in 3 seconds the PS LED lits but PF LED not lit. Is there any mistake? sir plz stay online.......and help me.. AttachmentNC-PLC data Clearing steps.pdf (834 Downloads) |
9/30/2011 3:19 PM | |
Posts: 23 Rating: (0) |
Hello sir PLC s4 switch is in 0 position PLC reloaded with s4 in 0 position yes plc archive is for same machine.... |
9/30/2011 3:36 PM | |
Posts: 23 Rating: (0) |
Sir AttachmentNC-PLC data Clearing steps.pdf (842 Downloads) |
9/30/2011 3:45 PM | |
Posts: 23 Rating: (0) |
Sir Is this the only reason for all these alarmsand LED 's blinking? i mean after nck and plc reloading this proble will be solved..... |
Follow us on