6/21/2015 6:10 PM | |
Posts: 7 Rating: (0) |
here is an other pic |
6/21/2015 7:13 PM | |
Posts: 7 Rating: (0) |
here its 6 |
6/21/2015 10:44 PM | |
Posts: 7 Rating: (0) |
it is on 6 all the time and is still giving the alarms |
6/26/2015 6:40 PM | |
Posts: 110 Rating: (3) |
HIU_d65Do you have solved your problemAli Rana
|
7/1/2015 5:36 PM | |
Posts: 7 Rating: (0) |
we tried that and it works fine but when we tried to change a tool it gave as another alarm 510100 tool torret 1 not ready and 510118 tool torret not indexed now any sug |
7/1/2015 6:54 PM | |
Posts: 110 Rating: (3) |
Hi dear U_65f 1st tell me that do you restore Machine backup or which procedure you removed alrams, if restore machine backup than do you clear PLC and NC Properly? and Plz tell me make or type of Turret and no of tools Alram no 510100 and alram no 510118 are related to turret hardware (mchanically problem) If Your turret is sample than check that motor movement if not then check the cables connection and power signal.if ok then you check phsically with out power that turret are properly locked.(clamped) may be it is unlocked ,if properply lock and positioned , After that you call tool no 01 (any) but not same come than you need to set 1st sequance of tools position therefor for this you need to check motor working condition is fine.if ok then check the tool turret position that turret properly unlock (unclamped) if not than check sensor or Limit switch position (Unclamped position) if you think that turret switches ok or not proper unclamped then check solenoid value.if ok and you feel it stop before clamp (lock) position then you need to phesically (mechanically) adjustment. Same procedure for clamped Problem. also a sensor is used for clamped position.Check it position hope full if turret is sample not a magzine then it give good help with best hope Rana Ali |
Last edited by: Rana Ali at: 7/1/2015 7:05:14 PM |
|
7/1/2015 7:43 PM | |
Posts: 7 Rating: (0) |
the machine in niles simmons n30
we cleared the plc with the s4 switch and afther that we load the backup from the archive |
Last edited by: U_d65fbc64-c1e6-420a-90e2-dd1957a662de at: 7/1/2015 7:45:38 PMLast edited by: Min_Moderator at: 7/2/2015 9:19:23 AM |
|
7/1/2015 8:13 PM | |
Posts: 110 Rating: (3) |
ok Alram no 510100 and alram no 510118 are related to turret hardware (mchanically problem) check that motor movement if not then check the cables connection and power signal.if ok then
you check phsically with out power that turret are properly
locked.(clamped) may be it is unlocked ,if properply lock and positioned
, After that you call tool no 01 (any) but not same come than you need
to set 1st sequance of tools position therefor for this you need to
check motor working condition is fine.if ok then check the tool turret
position that turret properly unlock (unclamped) if not than check
sensor or Limit switch position (Unclamped position) if you think that
turret switches ok or not proper unclamped then check solenoid value.if
ok and you feel it stop before clamp (lock) position then you need to
phesically (mechanically) adjustment. Same procedure for clamped
Problem. also a sensor is used for clamped position.Check it position are you sure that no accident happen with turret,if happen then you need to adjust mechanically setting with best hope Rana Ali |
7/3/2015 4:48 PM | |
Posts: 9 Rating: (0) |
Hi All, I am using 810 D CNC System. It is showing continuously & segment LED status 3. Even after tried all reset with S3 and S4 . Pls help me out. I followed the complete procedure mentioned in DOCOn manual. Regards Mayank vaidya |
7/3/2015 8:57 PM | |
Posts: 7 Rating: (0) |
Rana Ali thank for all your help i found a manual for mechanikly locking the turret to position and now the machine is working fine but now i have an problem :) i am the one ho have to operate on the machine and i only have knolage of fanuc 6t op sys on mazzak slunt turn 25 i found some simulators and tutorials but all of them are for 808 nothing about 840d i only need to know how to measure the tool and to set the zero point of the workpice on the simulator (808 for pc ) is easy but on the 840d on the machine i cant find any button for measuring can you please help me with that and again thank you for everything |
Follow us on