11/4/2015 12:45 PM | |
Posts: 2 Rating: (0) |
Normal
0
false
false
false
EN-US
X-NONE
X-NONE
MicrosoftInternetExplorer4
Dear experts, I m new to the STL programming and I have a problem that I can not solve. I'm working on a program that controls the temperature in the 10 rooms. Every room has three inputs: for room one: IW10 reference temperature value, IW12 measurement, IW14 work mode (0-heating, 1 cooling is send at bit 4) and two outputs QW10-heating,QW12 cooling. For room two IW16 reference temperature value, IW18 measurement, IW20 work mode (0-heating, 1 cooling) and two outputs QW14-heating (also bit 4),QW16 cooling (also bit 4) and so on to room 10. I am also calculating the number of rooms with present people in front of the total number of rooms which are empty. I have attached my program and would be grateful if someone would tell me what I'm doing wrong. Thank you in advance AttachmentSlavko_Batinic_Project.zip (74 Downloads) |
11/5/2015 5:27 PM | |
Posts: 8946 Rating: (999) |
Nobody like to do your homework. Please explain us what your problem is and what do you try to find a a solution. |