11/16/2023 6:15 PM | |
Joined: 11/8/2017 Last visit: 5/21/2024 Posts: 318 Rating: (175)
|
Hi, The RXB controllers need to be programmed / downloaded before they will work. As they are KNX-communicating controllers, this should ideally be done with the ETS tool (KNX software). It's been several years since I last worked with RXB controllers, but this is the tool I used. Another possible option (that I know nothing about) is the ACS tool from Siemens - see HERE. It's also possible to use a Siemens QAX34.1 to change some of the parameters, however this may well be a discontinued product. Regards, |
Follow us on