17.06.2014 16:20 | |
Beigetreten: 30.07.2007 Letzter Bes: 02.09.2024 Beiträge: 20 Bewertung:
|
Bis zum "Reboot" komme ich bei meiner Installation gar nicht! Hier das Installation-LOG. Wer kann mir sagen was das schief läuft? 2014.06.17 15:38:41 - Year.Month.Day - Log start BUNDLE: SIMATIC STEP 7 Professional V13.0 SEBU Version: PROFESSIONAL:TIA.rgs.RTM_13000000:V13.00.00.00_15.07.00.01 OS: Microsoft Windows 7 Enterprise Enterprise Edition, Service Pack 1, 64-bit, build 7601 COMMANDLINE: C:\Program Files (x86)\Common Files\Siemens\Automation\Siemens Installer Assistant\305\SIA2.exe /starter /bundlepath=G:\InstData INSTALLDIR: C:\Program Files (x86)\Siemens\Automation SETUPLANGUAGE: 1031 CHANGES: (+)DotNet_Updater;(o)CONFSQL2008R2EXP;(+)NCMGPRS64;(+)SECON;(+)S7DOS64;(+)S7DOS;(+)S7EDB;(+)PlcSim64;(+)PLCSim;(+)WinCC Runtime Advanced Simulator;(+)PTSymLib;(+)AlmPanelPlugin64;(+)Prosave There are NO severe messages before the installation 15:38:41 | BEGIN. Execution started. 15:38:44 | OK RunningProcesses (), Complete 15:38:45 | OK InventoryBefore (A), Complete 15:38:45 | OK Citamis (Before), Complete 15:38:45 | OK ClassicCompPrepare (), Complete 15:38:46 | OK ProductRegistration (Before), Complete 15:38:46 | OK ClassicCompAfterUninstall (), Complete 15:38:47 | OK SetupUnit (DotNet_Updater), Complete - - Foreign, AddLocal 15:38:48 | OK SetupUnit (CONFSQL2008R2EXP), Complete - - ClassicProduct, Reinstall 15:38:49 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:38:49 | FAIL! SetupUnit (NCMGPRS64), Failed - - ClassicComponent, AddLocal 15:38:50 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:38:50 | FAIL! SetupUnit (SECON), Failed - - ClassicComponent, AddLocal 15:38:56 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:38:56 | FAIL! SetupUnit (S7DOS64), Failed - - ClassicComponent, AddLocal 15:38:58 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:38:58 | FAIL! SetupUnit (S7DOS), Failed - - ClassicComponent, AddLocal 15:38:59 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:38:59 | FAIL! SetupUnit (S7EDB), Failed - - ClassicComponent, AddLocal 15:39:00 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:39:00 | FAIL! SetupUnit (PlcSim64), Failed - - ClassicComponent, AddLocal 15:39:26 |ERROR AdsWorkerClassicProduct::OnWorkerCompleted(): - ClassicProduct setup result: : 15:39:26 | FAIL! SetupUnit (PLCSim), Failed - - ClassicProduct, AddLocal 15:39:27 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:39:27 | FAIL! SetupUnit (WinCC Runtime Advanced Simulator), Failed - - ClassicComponent, AddLocal 15:39:33 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:39:33 | FAIL! SetupUnit (PTSymLib), Failed - - ClassicComponent, AddLocal 15:39:36 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 15:39:36 | FAIL! SetupUnit (AlmPanelPlugin64), Failed - - ClassicComponent, AddLocal 15:40:01 |ERROR AdsWorkerClassicProduct::OnWorkerCompleted(): - ClassicProduct setup result: : 15:40:01 | FAIL! SetupUnit (Prosave), Failed - - ClassicProduct, AddLocal 15:40:01 | OK ClassicCompAfterInstall (), Complete 15:40:01 | OK ClassicCompRollback (), Complete 15:40:04 | OK HspInstall (), Complete 15:40:05 | OK ProductRegistration (After), Complete 15:40:06 | OK SetupIsComplete (), Complete 15:40:06 | OK InventoryAfter (Z), Complete 15:40:07 | OK LicenseTransfer (), BeforeStart 15:40:07 | OK Citamis (After), Complete 15:40:07 | OK SetupSummary (), Complete 15:41:07 | OK SetupReport (), Complete 15:41:07 | END. Execution completed. Exit code: 1603 Errors: 11 Warnings: 0 Exit code means: Installation failed (InstallFailure) |
Zuletzt bearbeitet von: Narrator1 am: 6/23/2014 10:28 AMThema gesplittet von /tf/WW/en/Posts/109878#top |
|
18.06.2014 13:49 | |
Beigetreten: 30.07.2007 Letzter Bes: 02.09.2024 Beiträge: 20 Bewertung:
|
Hallo Christoph, hab das vollständige Installation-Log angehängt. Und ja, auf dem W7-64Bit Laptop läuft die Step7 V5.5 SP4 einwandfrei, obwohl die "SIMATIC Device Drivers WoW.msi" angeblich nicht installiert werden konnten. Das TIA V12 SP1 läuft auch, aber bekanntermaßen sehr langsam. Im Logfile hab ich 9 Eintrgäge gefunden mit dem Titel "ClassicProduct setup failed due to unknown error" - das betrifft: Step completed: SetupUnit (NCMGPRS64), Failed - - ClassicComponent, AddLocal Step completed: SetupUnit (SECON), Failed - - ClassicComponent, AddLocal; Step completed: SetupUnit (S7DOS64), Failed - - ClassicComponent, AddLocal Step completed: SetupUnit (PlcSim64), Failed - - ClassicComponent, AddLocal Step completed: SetupUnit (PLCSim), Failed - - ClassicProduct, AddLocal Step completed: SetupUnit (WinCC Runtime Advanced Simulator), Failed - - ClassicComponent, AddLocal; Step completed: SetupUnit (PTSymLib), Failed - - ClassicComponent, AddLocal; Step completed: SetupUnit (AlmPanelPlugin64), Failed - - ClassicComponent, AddLocal; Step completed: SetupUnit (Prosave), Failed - - ClassicProduct, AddLocal Aufgrund dieser Fehlerhaften Installation lässt sich zwar TIA in der Portalansicht öffnen, aber beim wechsel in die Projektansicht stürzt es ab. Habe TIA V13 jatzt schon 2 deinstalliert und danach wieder installiert - immer mit dem selben Ergebnis. Kann man denn beim Upgrade von V12 => V13 etwas falsch machen? ausser DVD rein und "start.exe" doppelklicken? Ich weiß nicht mehr weiter. Bitte helft mir. Gruß Burkhard DateianhangSIA_STEP7_PRO_V13@14-06-18_12-30-33_log.pdf (194 Downloads) |
Zuletzt bearbeitet von: Heiser71 am: 18.06.2014 13:50 |
|
23.06.2014 10:40 | |
Beigetreten: 22.07.2008 Letzter Bes: 14.04.2022 Beiträge: 1884 Bewertung:
|
RIP |
Zuletzt bearbeitet von: 1test am: 08.06.2016 13:41:49~(‾▿‾)~ |
|
Folgen Sie uns auf