1/18/2020 11:23 AM | |
Joined: 12/27/2018 Last visit: 7/19/2024 Posts: 510 Rating:
|
1.Delete the alarm log file.You don't have SD Card, but log file might be saved somewhere internal memory. 2.Delete "simatic" folder from internal memory ,program folder" and the reset once again via prosave TIA. 3.Compile and rebuild the project and download it.Use latest version of TIA Portal which you have in laptop. 4.Update OS 5.If problem persist, make a new simple program and download to HMI. This program shall smaller size.Then check the behavior of the HMI. If HMI again reboot then infer that HMI have component problem or virus infection. |
Jinson Kurian Vilayil James, P.Eng, BE, M.Tech (Power Electronics and Power System),PGDM, MBA |
|
Follow us on