10/15/2021 10:24 AM | |
Posts: 257 Rating:
|
Hello SIOS forum community, We keep receiving questions about which attributes can be read or written automatically using TIA Openness, e.g. whether write protection can be set or removed for all FBs. In the current TIA Portal Openness version, the attribute "isWriteProtected" is declared as ReadOnly. Specifically: Via the API (interface for programming applications), it can be read out whether the programme block is write-protected, but its value cannot be changed. Whether individual attributes can be edited via TIA Portal Openness is usually already listed in the instructions for the API. Further information can be found in the online help of Siemens TIA Portal. It is also worth taking a look at the TIA Openness Explorer. This lists all available attributes including access (read, write). Further information on the topic of TIA Openness: TIA Portal Openness: Introduction and Demo Application SIMATIC TIA Portal Openness: Automating creation of projects Tool for easier use of the TIA Portal Openness interface (Openness Scripter) Best regards, SIMATIC International Technical Support Hub |
This contribution was helpful to
1 thankful Users |
Follow us on