3/27/2009 8:42 AM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating:
|
Hi Here are thereplies of your requests: 1. The only way to connect the panel with the PG it is to use a serial cable. 2. The data exchange betweeen the PLC and OP17 can be proceeded via MPI. But youcannot upload and downloadfrom the PG to the OP via MPI. 3. Look to the first and second reply. 4. Set the operating unit to Download mode: During startup with the key combination ESC + cursor (OP 7 and OP 17 only), or by means of a general reset ESC + cursor > + cursor ¯ Maybe the following FAQ will help you: http://support.automation.siemens.com/WW/view/en/19109408 The manual of the OP17: http://support.automation.siemens.com/WW/view/en/1145112 Bye |
Follow us on