8/10/2022 12:36 PM | |
Joined: 5/12/2006 Last visit: 10/9/2024 Posts: 22405 Rating: (3017)
|
Openness is a API not a program. so you must write your own program and use the Openness API to get what you want. TIA Portal Openness: Introduction and Demo ApplicationTool for easier use of the TIA Portal Openness interface (Openness Scripter) |
8/10/2022 4:54 PM | |
Joined: 3/30/2020 Last visit: 10/9/2024 Posts: 4837 Rating: (988) |
Hello. Have a look at this conversation: OpennessScripter can be downloaded from.. Export to an ascii text file is available when PLC code is in SCL. The actual base case is that you have a generic building block (FB / FC) that is parameterized by linking the input and output pins to the relevant inputs/outputs/configurations. The building block is repeated for each machine part (like: conveyor). The filled in parameters makes it custom for the machine part. The HMI has the same concept if you use a Comfort or higher visualization system (HMI / Scada). There the use of 'faceplates' is available. Whatever you export, the modified and re-imported coding sound give the base case of multiple used building blocks. Perhaps supply more detail of what you have and what you want to do. Are you building one or thousands of the same variation? Mention which hardware is involved in the design. Why do you mention a "backup"? Is this someone else's work? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
8/11/2022 8:39 AM | |
Joined: 10/11/2017 Last visit: 3/28/2023 Posts: 13 Rating: (0) |
Thanks K_Ohjus, Any further queries related to C# ll post. |
Follow us on