9/26/2022 5:30 AM | |
Joined: 3/30/2014 Last visit: 8/8/2023 Posts: 83 Rating: (0) |
I'm afraid I've ruined my entire project. Somehow the wiring was wrong. This one is correct now. In the meantime I was able to fine-tune the fixed IP addresses. To be on the safe side, I just got a new LOGO! bought for control. Is a version 8.3 now. But he's doing his job somewhere. But now new problems are emerging. I am unable to make a connection between the meter box and the control. When I want to make a connection, I always see a black circle with a line through it. Same with the connection to "boiler". Here I can no longer connect to B014 either. However, it has always worked. Grid PWR may have succeeded, but it just took over. Meterkast (meter box) controle (control) B006 -> B006 B004 -> B008 Any idea why this happened? AttachmentHoefsmid10.zip (426 Downloads) |
Last edited by: Tcmatik at: 09/26/2022 05:35:47Last edited by: Tcmatik at: 09/26/2022 05:49:11 |
|
9/26/2022 5:59 AM | |
Joined: 3/30/2014 Last visit: 8/8/2023 Posts: 83 Rating: (0) |
"Allow S7 access" is on. |
9/26/2022 6:33 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
Try this.
AttachmentHoefsmid10_V2.zip (371 Downloads) |
9/26/2022 7:10 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33500 Rating: (4162)
|
I deleted the NAIs and the NAQs and wired via Drag & Drop without problems. |
Follow us on