3/21/2024 12:09 PM | |
Joined: 2/16/2020 Last visit: 4/26/2024 Posts: 7 Rating: (0) |
I'm having trouble registering this "musicDLL.dll" in Window 10. I've migrated the WinCC Flexible 2005 SP2 project that was on an XP computer to WinCC Flexible 2008 SP5 on a Windows 10 computer. I get an error stating the registering of the DLL fails. I don't have a copy of the message right now but can get it and later attach to this post. But it does refer to a potential problem could be that it is not compatible with Windows 10 OS. Has anyone been able to have this DLL registered in Windows 10 (or 11) to get a speaker to sound an alarm? Everything else works fine but I can't get the sound to be produced . Opening the wav file will make the sound at the speaker OK. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/22/2024 09:28:26New subject after splitting |
|
3/27/2024 9:01 AM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello Carrot Top I recommend using the latest Update for WinCC flexible 2008 SP5 that is available: https://support.industry.siemens.com/cs/ww/en/view/109757233 To play sounds you can try this: https://support.industry.siemens.com/cs/ww/en/view/26106312 Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/2/2024 5:42 PM | |
Joined: 2/16/2020 Last visit: 4/26/2024 Posts: 7 Rating: (0) |
Thanks Bye Murof, but I was hoping not to edit the project by writing new script. The original project had a DLL file created by MikePC with the Win XP version of WinCC Flexible 2005. I read a post to his by Alexey_Atyran that indicated it worked for a TIA project that I would assume is on a Win 10 PC OS. I believe that the DLL file might only be compatible with XP as to why I can't register it to use the original method of sound and cancelling an alarm. He may have solved that issue but haven't heard from him on a personal message a week or so ago. But thanks for your post to this issue Also, I've attached the windows message I got (and note that the Bye2008 has the Update 2) Carrot Top Attachmentscreen shot.pdf (4 Downloads) |
Follow us on