3/22/2021 11:40 AM | |
Posts: 2 Rating: (2) |
Hello everyone, I am working on a Scada project using Wincc unified TIA 16 1- I opened wincc unified configuration, I configure it and wait until it show everything done. 2- I run simulation for my project 3- I opened simatic runtime manager to check my project is run 4- I open my browser and write (https://localhost/) then I click enter 5- then I click wincc unified runtime 6- after I click that button it did not open the page of logging user and passwords but show there is an error Swaclogin is unavailable kindly check the attached image please support thanks abdallah abdeen ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/22/2021 13:53:19New subject after splitting |
|
3/27/2021 1:59 PM | |
Posts: 2 Rating: (2) |
After 1000 trials to find a solution and searching online, I tried to think simply. I solved this error by selecting the appropriate windows features. you can find it by checking the following link: https://support.industry.siemens.com/cs/ww/en/view/109773589 As an automation engineer, Siemens is part of my life. Regards, Abdallah Abdeen Egypt |
Last edited by: abdallah abdeen at: 03/27/2021 14:00:57Last edited by: Jen_Moderator at: 03/29/2021 11:19:32Optimized link. |
|
This contribution was helpful to5 thankful Users |
3/1/2022 8:53 PM | |
Joined: 8/10/2021 Last visit: 7/30/2023 Posts: 15 Rating: (0) |
Hello , i did all steps in the Link but however, the same message still appears, do you have another idea. |
5/9/2024 6:14 AM | |
Joined: 6/14/2011 Last visit: 5/17/2024 Posts: 3 Rating: (0) |
I am using TIA V19 and WinCC unified, facing issue of Swaclogin is unavailable error. SOLVED: Issue is resolved by switch off/disable the proxy server ( In Windows 11 OS -> Network & Internet > Manual proxy setup > Under Edit proxy server switch off proxy server. Refer attachment for error details and proxy server settings. AttachmentProxy server settings.zip (23 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on