9/12/2024 2:08 PM | |
Joined: 3/20/2024 Last visit: 10/8/2024 Posts: 1 Rating: (0) |
Hello I am trying to connect to an OMRON Print Server API using the function LHTTP_PostPut but continually get the Error Status 8601 which points to the TSEND_C status of 809A 'The CONNECT parameter points to a field that does not correspond to the length of the connection description.' I cannot figure out what is causing this issue. I have tried the command using POSTMAN and this works. I am also using the same information I can see sent by POSTMAN in the console. See API Picture 1 which shows the status and the data in the DB. URL : 'http://127.0.0.1:8084/api/printinspection/automation/v1/security/login' ContentType : 'application/json' userFields : 'Authorization: YWRtaW46YWRtaW4=$00' This all matches up with POSTMAN data sent see API Picture 2, that I can tell. I am testing using TIA Portal V19 and PLCSIM Advanced on the same machine as the API. Has anyone got any pointers as to where the issue is? AttachmentAPI Picture.zip (255 Downloads) |
Last edited by: AutoGen_7538895 at: 09/12/2024 14:35:34 |
|
Follow us on