9/13/2024 5:50 AM | |
Joined: 8/3/2009 Last visit: 10/18/2024 Posts: 13982 Rating: (1760)
|
Hello AutoGen_8317281 You have to use a different accesspoint in PGPC Interface. So it depends on which PLC type you use... with a S71200/1500 it works because you can use a different Access Point but if you have all PLCs as s7-300/400 then this will not work, because the TCPIP Channel of S7Protocol Suite has only one Accesspoint in Case of a S71500/1200: Open the SetPGPC Interface in Control Panel, create a new one and set it with your networkcard for the connection4 Set this Accesspoint in the connection setting of your PLc Connection in winCC (I know its not WinCC V7 but in this FAQ you can see how to use different Accesspoints, only the dialogs in WinCC looks a bit different but the way is the same) Bye Murof |
Last edited by: Murof at: 09/13/2024 05:53:17If this Information really helps, you could use the Rate function |
|
Follow us on