11/12/2009 1:00 AM | |
Joined: 1/4/2008 Last visit: 2/27/2024 Posts: 703 Rating: (96) |
Hello Deka, from the product support page: SIMATIC WinCC only supports the operating system languages German, English, French, Spanish and Italian. You need the SIMATIC WinCC ASIA language version for Asian operating system languages (Chinese Traditional, Chinese Simplified, Japanese, Korean). SIMATIC WinCC ASIA can be used in the local operating system language in each case and in Windows XP MUI. More detailed information is available in the delivery release in Entry ID 21897202. As I know the Asia version includes also English so think if only the Englishis used in the project, it can be managed in standard version also in the Asia version, but haven't tested it. Regards Sydney |
Follow us on