1/19/2010 11:24 AM | |
Posts: 103 Rating: (11) |
how are you all, I have 2PCs , I want the following , 1st PC :computer name (ETGENG061) , with winccflexible installed on it , I WANT TO MAKE IT SERVER 2nd PC :computer name (ETGENG06) , with winccflexible installed on it , I WANT TO MAKE IT CLIENT I have logged on this FAQ https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=31198863&objAction=csOpen&nodeid0=16502374&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW I have executed all steps word by word , I have downloaded the sample projects in the FAQ and opened it on my PCs. my problems in client PC: 1) first picture : I don't have tree to choose symbol from it. but there is RED TRIANGLE. when you ask about the symbol already exists in the picture , I will say this symbols already added by SIEMENS programmer. now when I want to add any symbols , I CAN'T!!! 2)second picture : I don't have tree at ETGENG061 (SERVER) to choose OPC SERVER NAME from it someone may recommend to check connections between 2 PCs 1) i use cross over ethernet cable between 2 PCs 2)I opened START>>RUN>> write PING (another computer IP), the result is the PC sent and receive successfully, this result repeated in two PCs . hint:- I have no PLC right now , but I use simulation so I have downloaded PLCSIM OPC , made setup for it and write IPs of server and client PCs as shown in the pictures in the attachments please help me to solve this problems thanks AttachmentDCOM.zip (166 Downloads) |
Last edited by: ahmedmae94 at: 1/20/2010 8:13 AM |
|
1/21/2010 2:49 PM | |
Posts: 5822 Rating: (411) |
Hello, I admit this is a really tough subject you may spend a lot of time with. First of all I would recommend to you to try this document, which is part of the WinCC flexible CD. You may find it at the directory: <your CD Drive>:\CD3\Support\OPC\ Check it out. Best regards J_Bell AttachmentOPC_via_DCOM.pdf (209 Downloads) |
1/27/2010 9:46 AM | |
Posts: 103 Rating: (11) |
thanks , thanks , I feel we are near to solve the problem , <<<Would you have a WinAC installed instead at your PC you would be in a much easier situation>> yes , and the pictures in the attachment shows that , but i don't know how to use this software . please help me to learn it ////////////////////////////////////////////////////////////////////////////// <<Did you ever try to check theexistence of your Free PLCSIM OPC Server as an object in the COM area of your local PC and if it is detectable form remote by the use of some DCOMCFG or some OPC Client applications?>> yes , detected in both PCs , the pictures in the attachment shows that. ///////////////////////////////////////////////////////////////////////////// <<does your PLCSIM OPC Server work with Libnodave?>> what's the meaning of Libnodave ?? thanks in advance. AttachmentOPC_detected.zip (155 Downloads) |
1/27/2010 10:07 AM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating: (1159)
|
Dear ahmedmae94, Sorry to interrupt the discussion , but perhaps here are some links, with more information about WinAC: how do you configure communication between the WinCC flexible Runtime and WinLC via Softbus on a PC? WinAC RTX -- Configuring and programming communication -- Configuring communication to S7 What connections are there between the version designations in WinAC RTX? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
1/27/2010 1:38 PM | |
Joined: 4/24/2006 Last visit: 6/14/2024 Posts: 8683 Rating: (1159)
|
Dear ahmedmae94, Perhaps this link, might give you some information about the difference between WinAC and WinAC RTX: http://support.automation.siemens.com/WW/view/en/6919918 Well, instead of using PLCSIM OPC, you could use WinAC RTX as a CPU to connect to. The WinCC flexible RT 'Server' could connect to WinAC RTX and should be an OPC server for the other WinCC flexible RT 'Client'. Best regards, Wizard |
Follow us on