2/3/2011 10:57 AM | |
Posts: 4 Rating: (0) |
Hi friends, 1. Complete back up of my working OP170B is taken.The file is saved as a PSB file.I tried to download it to a spare OP170B, but it was givingone warning like "all licence will be deleted or overwritten" something like that.Can I continue it?I didnt find any licence CD in the OP consignment recieved from Siemens.Whats the usual procedure? [schnippschnapp] second question is splitted to If I switch over the TP mode to Transfer mode for Complete Back Up using Prosave,will the CPU also go to stop mode?. Please help me in clearing my doubts. Regards, Friend |
Last edited by: O_Moderator at: 2/3/2011 12:58 PM |
|
2/3/2011 11:13 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Make resetting to factory settings. How do you do an operating system update (OS update) on operator panels? |
Follow us on