7/11/2011 11:23 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
In PLC, there are several to measure the elapsed time; more information about that here: Hour counter with LAD of FBD Using SFB3(TP),SFB4(TON)and SFB5(TOF) is much easier to create an application in PLC.I think TON can provide the running time of pupm in #TIME format and it can be transferred to WINCC and also interpreted there.Try it, update if there is any difficulties! |
This contribution was helpful to1 thankful Users |
7/11/2011 5:29 PM | |
Posts: 59 Rating: (0) |
also time to start where they left off. best regards
|
Follow us on