11/24/2011 12:01 PM | |
Posts: 5225 Rating: (1196) |
TESTED BUT FAILED
Pegaia, Thank you for the effort. I am however having trouble to open the project correctly. First my version was not right.. I did not have UPDATE 2 loaded. So I did that first. Now I get a very strange error message - the system requesting WinCC SP1 Update2. According to the install version status window this is what is installed. See the JPG for details. I notice however that you have used a TP1200 Comfort as panel and not the Basic Panel. Again refer to the JPG. I think the problem is that TIA BASIC does not handle the TP1200 Comfort. Why the error message does not just say I require TIA Professional, is an open question. [wink+smile] Maybe I should get a sponsor for buying me TIA Professional.. I seem to be the only one with TIA Basic wanting to see inside this program. Hope this feedback helps. |
12/20/2011 12:10 PM | |
Posts: 3037 Rating: (192)
|
Hello Simon N, What do you use acknowledge about PLC or acknowledge about HMI? You can see more information for alarms in the following manual. See chapter 9.3.2 Working with alarms. WinCC Comfort / WinCC Advanced V11.0 SP1 Tweety |
Follow us on