6/10/2012 9:46 AM | |
Joined: 9/12/2011 Last visit: 5/25/2024 Posts: 61 Rating:
|
hiandreazana, try to adjust the transfer protocol in the TP177B ... after booting the panel goto control panel and open (Transfer menu) then choose it to be ETHERNET and right down the IP address ... then close control panel and put the panel in transfermode ... then in winCC write the Panel IP address in transfer window ... It will work ...
|
George Awny |
|
6/10/2012 12:05 PM | |
Joined: 8/31/2010 Last visit: 6/24/2024 Posts: 1516 Rating:
|
Hello andreazana, First try disabling the ethernet interfaace of your PC and enable it again, it may sound quite funny but it has worked out for me most of the time. If it still doesn't work then I'm not aware if you are using WinCC based on TIA Portal or WinCC Flexible. If you use TIA Portal based WinCC then refer this below procedure for transferring configuration to panel thro' MPI/PROFIBUS and Ethernet - How can you transfer a WinCC (TIA Portal) configuration to an operator panel using MPI/PROFIBUS? - How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? If you use WinCC Flexible then refer this below procedure for transferring configuration to panel thro' MPI/PROFIBUS and Ethernet - How can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? - How can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? - How can you transfer a WinCC flexible project serially to a panel? - How can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this? |
Like it? Rate it! |
|
This contribution was helpful to
1 thankful Users |
6/12/2012 2:59 PM | |
Posts: 3037 Rating:
|
Hello andreazana, this link is useful for the download to a panel. You can see alltarnsfer optionsand information about cables. What transfer options are available in the various operator panels? Tweety |
6/13/2012 9:02 AM | |
Joined: 5/28/2008 Last visit: 6/27/2024 Posts: 4510 Rating:
|
Hello, Yes, someone can disable ethernet port when you are not arround of your Panel. Control panel is accessable during booting the panel. What you should to do every time when you download/upload project to the panel is to follow the instructions as given in the above links of Ganis10. See page 5 of the attachment ofHow can you transfer a WinCC flexible project via Ethernet to a Windows-based panel? Also see page 20 of the attachment ofHow can you transfer data via USB from a WinCC flexible configuration computer to a Windows-based operator panel and which USB cables can be used for this? To conclude; You have always to check if the transfer port you want to use is enabled or not. Hope this helps.
|
Ayman Elotaify |
|
Follow us on