12/5/2013 2:52 PM | |
Posts: 46 Rating: (0) |
Dear Grad, answer to your questions: 1. Never tried it before 2. I have a counter that sets a bit 3. I have not, since this is my first MODBUS encounter. Please refer to the following link : Best regards, |
12/5/2013 4:01 PM | |
Posts: 6 Rating: (0) |
Ok, here is a tool i suggest you get in order to double-check you client. I will have a look at your code. http://www.modbustools.com/modbus_slave.asp |
12/5/2013 6:46 PM | |
Posts: 6 Rating: (0) |
OK, Go retrieve this one and try it. Use PLC22 to talk to your device. See the Comment in the Client Network. You must use Un-Optimized DB as the Variant. https://tsuoad.box.com/s/bfb5kphv7a0et2xo9ekm |
This contribution was helpful to1 thankful Users |
12/6/2013 9:18 AM | |
Posts: 46 Rating: (0) |
Dear GRAD, thank you for your time. It does not work, I get no data. I have tried changing the address to 40002, it still does not work. I tried disconnecting PAC3200 from switch. It shows no error. If I go to communicate with the PAC directly it works, but trough this MODBUS_CLIENT it does not work. Could you explain what un-optimized DB means? I looked at my project DB, and it is also not optimized. Could you explain MB_DATA_LEN 10, and array of integers for a DB?
|
Follow us on