10/5/2007 8:00 AM | |
Posts: 2348 Rating: (264) |
Look under http://support.automation.siemens.com/WW/view/en/16750732. You need memory card of appropriate size to do it. PS. Didn't find v3.0+.... |
10/7/2007 10:58 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
Hi, V2.6.3 is the newest firmware for the S7-315.... Please look under the next link: Operating System Updates for CPU 315-2DP or for the PROFINET CPU 315: Operating System Updates for CPU 315-2 PN/DP For older versions then V2.6.0 you have to use a MMC, for newer versions you can write the firmware directly to the CPU. Online: Prerequisites:
Durchführen eines Firmware-Updates:
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to2 thankful Users |
Follow us on