9/11/2014 1:10 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating:
|
Hello friends I am facing a peculiar problem, whenever I try to Send an archived project ( Zip ) to anyone with a GMAIL ID. It is rejected by the GMAIL Server with the following error : This message was blocked because its content presents a potential 552-5.7.0 security issue. |
There is no such thing as the last bug in a program |
|
10/15/2014 3:05 PM | |
Joined: 9/11/2012 Last visit: 9/14/2023 Posts: 43 Rating:
|
Hello Navnag It is not just the Gmail, but all email exchange servers have the same protocol for sending/receiving executable files. Like it is explained in the gmaillink pasted by you it is just a securitymeasure. The only way to deal with it is the one you already know. I take the liberty to put it in here for all our fellow members. It is not a siemens system limitation or a bug. To go around the system you can create multiple layers of zip files and then change the extension of these zip files before sending it. And askthe receiver of these files to change the extensions back to zip after receiving. Or use FTP websites as mentioned in the earlier reply. Hope it helps. Cheers Fredrick |
Last edited by: Fredrick D at: 10/15/2014 3:10 PMLast edited by: Fredrick D at: 10/15/2014 3:09 PMLast edited by: Fredrick D at: 10/15/2014 3:07 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on