9/29/2015 2:01 PM | |
Posts: 1 Rating:
|
Question. I am trying to use a Memory/Battery card for OBA6. The version is 6ED1056-7DA00-0BA0. In the old days you could put an memory battery card in to a siemens logo and load the program from the logo to the memory card. Now I have ordered 2 new cards witch won't work. When loading the program from the logo to the memory card it gives the messages Card Unknown. I tryed it with an old card and that one is still functioning. The code on the old card is 6ED1 056 7DA00-0BA0. The code on the new card is the same. What is happening here? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 9/30/2015 10:41:14 AMNew subject after splitting |
|
10/5/2015 11:25 AM | |
Posts: 2930 Rating:
|
Hi, try: swich OFF Power, then plugin the Card, then see if it works now. Hope this helps |
Follow us on