10/13/2016 1:10 PM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating:
|
Hi Miguel, at first you should check out the Ident Configurationg Guide: For reading over long distances (several meters) you will want to use RF600 (UHF) readers and transponders. In the configuration guide you can find all transponders available sorted by protection levels (IP codes) and reading distances. For high pressure and temperature you will want to look for transponders specified with IP class IPx9K. The RF600 readers can easily be integrated into the SIMATIC systems by PROFINET or various communicatin moduls. Also there are program blocks included into TIA Portal for commissioning the readers. For short distance reading operations you should use RF200 (HF) readers and ISO/ MOBY D transponders (RF600 could also be used for short distance, but its way more expansive). ISO/ MOBY D transponders are also available with IP protection class IPx9K. I hope this short overview is what you were looking for. Regards. |
11/10/2016 6:50 PM | |
Joined: 8/21/2014 Last visit: 8/30/2024 Posts: 1006 Rating:
|
New question published by hamdiovich is split to a separate thread with the subject Error in RFID block. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on