3/9/2017 10:15 AM | |
Joined: 6/22/2009 Last visit: 5/24/2024 Posts: 62 Rating:
|
Hi, Can I use a standard Ethernet Card in a standard PC for a single ended WinCC with S7-400H? If I use REDCONNECT @ the PC, it should be able to connect/switchover between the 2 CPUs? Please refer to the configuration attached. In this case, can I use SOFTNET Lean, which comes free with WinCC V7.2? Best regards AttachmentConfig.pdf (51 Downloads) |
Follow us on