8/15/2017 2:53 AM | |
Joined: 2/20/2014 Last visit: 10/8/2024 Posts: 396 Rating: (38) |
Hi there, I had configured the CMR2020 communication module to send sms when the LOGO Input 1 triggers the M1 of the LOGO base module. What i notice now is that the same message is sent multiples times (most of the time 2 sms messages, some other times, the number of same messages sent varies (more than 2 sms for one event). Which means the same message being sent repeatedly for one event. Can anyone advice on this matte on what could be the possible cause? Attached is the LOGO CMR related details. Thank you in advance. AttachmentLOGO CMR2020_2017AUG15.zip (157 Downloads) |
Follow us on