1/9/2018 10:32 AM | |
Joined: 1/8/2016 Last visit: 6/7/2024 Posts: 3 Rating:
|
Happy new year to everybody!! Has anybody installed the trial yet? I tried the s7pro /wincc advanced and the PLCSIM V15 did not intall. Think it is not included at all in the software although it is supposed to ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 1/9/2018 2:44:05 PMNew subject after splitting |
|
1/9/2018 7:11 PM | |
Joined: 1/8/2016 Last visit: 6/7/2024 Posts: 3 Rating:
|
many thanks my friend |
2/8/2018 3:34 PM | |
Posts: 19 Rating:
|
PLCSIM V15 does not work after install. It displayed a message "Cannot locate Step 7 V15 license (STEP 7 V15 application MUST be installed on this computer)." What I did to make it work. I have V14SP1 upd4 also installed on my PC. I started 2 two V14 projects with (Openness) PLC Simulations at the same time. I then started V15 project and attempted simulation when it warned me that 2 max. simulations are allowed. When I closed one of the V14 Simulations and then started V15 - Invoked the V15 PLC Simulation -- It worked from that point on! |
Follow us on