12/24/2016 5:43 PM | |
Posts: 1 Rating:
|
HI TO ALL, I want the software of operator panel OP-17DP 6AV3 617-1JC20-0AX1 to upload the program from pc to plc and the type or serial of the cable thank you, best regerds, osama ahmed ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/25/2016 10:07:53 AMNew subject after splitting |
|
12/24/2016 7:47 PM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating:
|
Hello,
1-You can upload the backup"image"file from panel to PC with ProSave software. This backup file is not editable and restore to the same type of panel. 2-The cable between PC and panel is: RS 232 "cross cable" as in the attached file. |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to
1 thankful Users |
12/27/2016 11:02 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, You need the software ProTool, best regards |
12/29/2016 3:47 PM | |
Joined: 5/28/2008 Last visit: 7/21/2024 Posts: 4514 Rating:
|
Hello, The mentioned OP is too old and is phased out from several years. https://support.industry.siemens.com/cs/ww/en/pv/6AV3617-1JC20-0AX1/pi back to your question, you want a software of operator panel OP-17DP "6AV3 617-1JC20-0AX1" to upload the program from pc to plc Program of OP is different than the program of PLC. If you would like to download program to PLC, please tell us type of it and we can help and tell you which software and adapter you have to use. If you would like to upload program from OP17, you can only upload an image (non-edittable) using a freeware software called "Prosave" and you can download it from the link provided by "Online Tech" You can use cable "6XV1440-2K.."; its pin assignment is here or using right angle adapter (1:1) according to the attached excel sheet. Using cross RS-232 cable (or what we called Null-Modem cable) is not listed in the cables used for downloading or uploading of OP17. And also Protool Pro is the configuration software we use to develop projects for OPs like OP17. You can not use it to upload an image from it. Another important note, when you are ready to upload the image, you should prepare the OP to transfer mode by pressing ESC + UP Arrow keys together during powering up the OP. Please see sheet 3-5 of this manual Hope this helps. Attachment19109408_wincc_flexible_projekttransfer_e.xlsx (573 Downloads) |
Ayman Elotaify |
|
4/25/2018 1:24 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by Dave2018 is split to a separate thread with the subject How to replace old panel with new Panel 6AV36I7-1JC20-0AX1 ?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on