2/9/2019 3:52 PM | |
Posts: 3 Rating: (0) |
Hi Georg, Please, I tried to scale from WinCC 7.2 HMI some transmitters but no good output. Please find attached screen shots from one pH Analyzer (AIT-004). We have already at AI module 12 mA, this means pH 7 (local indicator at AIT-004 is indicating pH 7). I did scale in HMI: PLC range: (4-20) mA and OS range (0-14) pH, as per project attached Set point and range list. No effect, it is showing on HMI (running mode) pH -3.5. I attached also FB and DB from PLC for this analyzer. Please give some guidance to solve this issue (In PLC block, FC 230 which is used for SCALE, is hidden, I cannot open).
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/11/2019 11:39:25 AMNew subject after splitting |
|
2/22/2019 5:44 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hi, in this case I would recommend to create a service request: https://support.industry.siemens.com/cs/ww/en/sc/2090 Regards |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on