8/3/2019 3:28 AM | |
Joined: 7/30/2019 Last visit: 6/11/2024 Posts: 1 Rating: (0) |
Como conectar un transmisor de 2 hilos al módulo? |
8/3/2019 5:18 AM | |
Joined: 12/18/2014 Last visit: 9/27/2024 Posts: 33845 Rating: (4206)
|
Hello ARG_Tincho, first welcome to the forum. This is a english speaking Forum. Please be so kind an write your next posts in english. You take the plus of the 24 VDC power supply of the AM2 module and connect to the plus connector of the transmitter. Connect the negative terminal of the transmitter to the current input of the AM2 module. See attachment.
AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 49.pdf (171 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on