6/20/2016 2:37 PM | |
Joined: 5/12/2006 Last visit: 10/9/2024 Posts: 22405 Rating: (3017)
|
Hello, no the basic panels have no Sm@rt functionality, this is only possible with the Comfort Panels.
Christoph |
This contribution was helpful to1 thankful Users |
2/16/2018 10:13 AM | |
Joined: 3/16/2014 Last visit: 10/14/2021 Posts: 120 Rating: (67) |
It is present since TIA 14.0 for Basic 2nd gen. with firmware 14.0+ (and PN interface...) |
2/5/2020 8:40 PM | |
Joined: 3/1/2019 Last visit: 9/4/2024 Posts: 17 Rating: (0) |
Is this true? |
4/3/2020 6:01 PM | |
Joined: 5/12/2006 Last visit: 10/9/2024 Posts: 22405 Rating: (3017) |
yes this is correct |
Follow us on