6/1/2020 5:30 PM | |
Joined: 12/28/2016 Last visit: 9/13/2024 Posts: 364 Rating: (6) |
I have 3 S7-1200 CPU and these three are controlling three separate pumps I want to Show the Status of the pump etc. as well as the analog feedback from these 3 pumps on 1 HMI I have created 3 connections in the HMI, changed only the PLC address and rest kept as it is the access point is the same is it the correct approach Attachmentconnections.zip (161 Downloads) |
Last edited by: qwemx at: 06/01/2020 17:35:46With kind regards... |
|
Follow us on