1/14/2019 8:39 AM | |
Joined: 5/27/2015 Last visit: 7/25/2024 Posts: 60 Rating: (27) |
Hi Ajaramillo, It is necessary to Update WinCC Audit to the latest version: V7.4 SP1 Update 1 https://support.industry.siemens.com/cs/de/en/view/109754946 In the release notes there is the following improvement listet: "Audit is improved to stabilize PASSDBRT during SIMATIC Logon." There were crashes of the PASSDBRT.exe which lead to an automatic logout when using SIMATIC Logon on a system with WinCC Audit. In my case the Update to the latest WinCC version (V7.4 SP1 Update 9): https://support.industry.siemens.com/cs/de/en/view/109762790 and the Update of WinCC Audit solved the issue. Greetings |
This contribution was helpful to1 thankful Users |
1/15/2019 6:37 PM | |
Joined: 9/27/2012 Last visit: 3/11/2022 Posts: 18 Rating: (5) |
Thank you so much!!! It works!!!! |
Follow us on